Technical FAQs

Ask a Question

Will a QO shunt trip breaker fit in the C4L200S?

Issue:
Compatibility of electrical accessories in an All In One device

Product Line:
Combination Service Entrance Devices

Environment:
Residential Metering

Cause:
Requirements for remotely disconnecting the meter service
 
Resolution:
The C4L200S can accept a QO shunt trip breaker. However, electrical accessories require an additional pole space, and this device only has 4 pole spaces, to accept two 2-pole main breakers. This will limit the C4L200S to accept only one 2-pole main breaker
Was this helpful?
What can we do to improve the information ?