Technical FAQs

Ask a Question

What is the standard lug kit for Powerpact L frame breakers?

Issue:
What is the standard lug kit for the Powerpact L frame 250, 400, and 600 A breakers?

Product Line:
Powerpact LDL LGL LJL LLL LRL

Resolution:
The standard lug kit for the Powerpact L frame breakers are as follows:

  • 250A - AL400L61K3 [(1) 2 AWG–500 kcmil Al; (1) 2 AWG–600 kcmil Cu]
  • 400A - AL600LS52K3 [(2) 2/0 AWG–500 kcmil Al or Cu]
  • 600A - AL600LS52K3 [(2) 2/0 AWG–500 kcmil Al or Cu]

These lugs also work on Powerpact D and Compact NSJ breakers.

Was this helpful?
What can we do to improve the information ?