Technical FAQs

Ask a Question

What is the part number for a N.O. isolated alarm contact for melting alloy overload relays?

Issue:
What is the part number for a N.O. isolated alarm contact for melting alloy overload relays?

Product Line:
Class 9999 Isolated Alarm Contacts, Type 8536S starters, Type S starters, 9065 overload relays

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
For a N.O. alarm contact that will close on alarm, you will need the 9999SO4
Was this helpful?
What can we do to improve the information ?