Technical FAQs

Ask a Question

Is the GV7AE11 auxiliary contact normally open or normally closed?

Issue:
Is the GV7AE11 auxiliary contact normally open or normally closed?

Product Line:
TeSys GV7 Accessories

Environment:
All Product Lines

Cause:
The Digest does not specify

Resolution:
The GV7AE11 can be either N.O. OR N.C.

For a N.O. contact, wire 11 and 14. For a N.C. contact, wire 11 and 12.
Was this helpful?
What can we do to improve the information ?