Technical FAQs

Ask a Question

What is the wire range for the lugs provided in the SR69064A Solar Ready Kit used with certain CSED panels?

Issue:
Application

Product Line:
CSED

Environment:
Application

Cause:
Verification

Resolution:
The two phase lugs provided in the SR69064A will accept (1) #2/0 - #6 Al or (1) #2/0 - #10 Cu conductors. The neutral lug provided will accept (1) #2/0 - 6 Al or Cu conductor.
Was this helpful?
What can we do to improve the information ?