Technical FAQs

Ask a Question

Are QO NEMA Type 1 Load Center covers available without an integral door?

Issue:
Product Features

Product Line:
Load Center

Environment:
Product Feature

Cause:
Verification

Resolution:
The only QO NEMA Type 1 Load Center covers that are not provided with an integral door that provide access to the circuit breakers would include the covers that are provided with the following load centers:
QO2L30S
QO2L30TTS
QO24L50TTS
QO24L70F
QO24L70S
QO24L70TS
QO35FM30TTF
QO35FM30TTS
QO612L100F
QO612L100S
QO612L100TF
QO612L100TS
QO816L100F
QO816L100S
QO816L100TF
QO816L100TS
QO148L125GF
QO148L125GS
QO403L60NF
QO403L60NS
All other QO NEMA Type 1 merchandised covers are provided with an integral door and are not available without the integral door.
Was this helpful?
What can we do to improve the information ?