Technical FAQs

Ask a Question

Can the J225X be used for an outdoor, rainproof application?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Environment:
Application

Cause:
Clarification

Resolution:
Yes, this device comes with a breather and drain kit (PKDB1) that can be field installed, for an outdoor, rainproof application.


CTA-ID : 2050957
Was this helpful?
What can we do to improve the information ?