Technical FAQs

Ask a Question

Can the external mounting brackets be replaced on a NEMA Type 12/3R, Type 12K or Type 4/4X/5 stainless steel Heavy Duty Safety Switch?

Issue:
Repair parts

Product Line:
Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The mounting brackets are welded onto the enclosure and cannot be replaced.
Was this helpful?
What can we do to improve the information ?