Technical FAQs

Ask a Question

Is replacement coil available for 8911DPSG43V02 series B?

Issue: Replacement coil available for 8911DPSG43V02 series B
Product Line:
Square D starter
Environment:
Starter
Cause:
There is a need to know if provision for coil is available .
Resolution:
Yes, 9998DA1V02, coil consumption is 56 VA inrush and 6 VA sealed, series B only, series C does not have replaceable coils.
Was this helpful?
What can we do to improve the information ?