Technical FAQs

Ask a Question

Are the 9012 Type G Machine Tool Pressure Switches Motor Circuit rated?

Issue:
Needs to know if 9012G carries a HP rating.

Product Line:
9012GD/GE/GF/GA/GC

Environment:
Products sold and used in the United States

Cause:
Product specifications for selection and use in the field.
 
Resolution:
Class 9012 single state pressure switches are control circuit rated devices used in pneumatic or hydraulic systems on a wide variety of machine and process applications to protect the equipment and control or monitor the system pressure. They are not motor rated.

Was this helpful?
What can we do to improve the information ?