Technical FAQs

Ask a Question

What are the repair parts for the CH362DS, series F6? (may be shown as F06)

Issue:
Repair parts

Product Line:
Safety switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The repair parts for the CH362DS, series F6 (F06) are as follows. No other parts are available.
Line Base Assembly - 4056603850 (arc suppressor not included)
Load Base Assembly - 4056604050
Line & Load Base mounting screw - 4020515101 (3 for line & 2 for load)
Arc Suppressor Assembly - 4056635550
Arc Suppressor mounting screw - 4020514501 (1 required)
Lug Assembly - 4025101652 (per lug, line and load)
Mechanism Assembly - 4056646950 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
Handle Coupling - 4056699850
Cover Interlock Defeat Coupling - 4056699750
Handle Assembly - 4056779850 (also recommend replacing Lockplate Gaskets)
Lockplate - 4056681201 (also recommend replacing Lockplate Gaskets)
Lockplate Gasket - 4050322802 (2 required)
Lockplate mounting screw - 2194918121 (2 required)
Ground Lug - 4025101652 - (2 total required)
Ground Lug Mounting Screw - 4020513503
Fuse Pullers - FPK0610 (1 required for switch)
Was this helpful?
What can we do to improve the information ?