Technical FAQs

Ask a Question

What are the dimensions of a NEMA size 3 starter with melting alloy overload?

Issue:
What are the dimensions of a NEMA size 3 starter with melting alloy overload?

Product Line:
8536 Type S Starters

Environment:
US Product Lines

Cause:
Can not find it in the digest

Resolution:
Please see attached PDF for dimensions.
Was this helpful?
What can we do to improve the information ?