Technical FAQs

Ask a Question

Will the ground-fault protection function of the LX and LE circuit breaker function without the 120 Vac Ground fault test circuit being supplied?

Product Line:
LX and LE Square D, Micrologic Series B
 
Resolution:
The ground fault does not require the Ground Fault Test Circuit to be supplied with 120 Vac over terminal 3 and 4 to function. The circuit only powers the ground fault test function which simulates a ground fault for testing purposes.
 
  Terminal Name
No. LX/LXI LE
1 Neutral CT (to X1) Neutral CT (to X1)
2 Neutral CT (to X2) Neutral CT (to X2)
3 Ground-fault Test 120 Vac Ground-fault Test 120Vac
4 Ground-fault Test 120 Vac Ground-fault Test 120 Vac
5 Reversed ST Restraint IN
6 Reversed ST Restraint OUT
7 Reversed GF Restraint IN or GF Alarm
8 Reversed GF Restraint OUT or GF Alarm Restraint
9 Reversed Restraint COMMON
10 Reversed COMMON CIM3F—RED
11 Reversed CIM3F—Black
12 Reversed Reversed
13 Reversed CIM3F—BLUE
14 Reversed CIM3F—ORANGE
15 Reversed  Reserved
16 Reversed  Reserved
 
 
Was this helpful?
What can we do to improve the information ?