Technical FAQs

Ask a Question

What is the torque requirement for the 1/4-20 mounting bolts used to attach the SN100FA to the circuit breaker enclosure?

Issue:
Technical inquiry

Product Line:
Circuit Breaker Enclosure

Environment:
Technical inquiry

Cause:
Clarification

Resolution:
The SN100FA mounting bolts used to connect the neutral assembly to the circuit breaker enclosure should be torqued to 50 - 90 In. Lbs.
Was this helpful?
What can we do to improve the information ?