Technical FAQs

Ask a Question

Can a QOL225 lug kit be used on a 125A, or lower, load center?

ISSUE:
Application

PRODUCT LINE:
QO and Homeline Loadcenter

ENVIRONMENT:
Applies to QOL225 lug kit.

CAUSE:
Verification

RESOLUTION:
The lugs provided in the QOL225 lug kit are too large for use on the 125A and lower load centers. There would also be inadequate wire bending space in the smaller load centers for the larger wire that the QOL225 lugs will accomodate.
Was this helpful?
What can we do to improve the information ?