Technical FAQs

Ask a Question

What is the replacement lug for the 600 amp, Powerpact L frame, I line breaker?

Issue:
What is the replacement lug for the 600 amp, Powerpact L frame, I line breaker?

Product Line:
Circuit Breakers

Environment:
Applies to the 400/600 amp I line, Powerpact L frame breaker.

Cause:
Replacement lugs needed for the L frame breaker.

Resolution:
Replacement lug kit number is: AL600LF52K3, quantity 3 per kit.  Wire size, (2) 3/0 awg - 500 kcmil AL or CU.

 
Was this helpful?
What can we do to improve the information ?