Technical FAQs

Ask a Question

XW - Does the battery temperature mV/C setting in the Custom battery menu apply to Hot, Warm, Cold?

No. When setting the temperature compensation value in the Custom Battery menu, this only affects the charge voltage when a battery temp sensor (808-0232-01) is used.
Was this helpful?
What can we do to improve the information ?