Technical FAQs

Ask a Question

Can you copy the configuration from one ATS48 to another?

Issue:
Can you copy the configuration from one ATS48 to another?

Product Line:
ATS48

Environment:
All models and serial numbers

Cause:
None

Resolution:
The only way to transfer or copy the configuration from one ATS48 to another is to use SoMove you can not use the remove HMI to copy the program. 
Was this helpful?
What can we do to improve the information ?