Technical FAQs

Ask a Question

How to get the ATV312 to restart at the last set frequency after the power has been cycled, when using up and down arrows on the speed reference or when using the plus and minus speeds?

Issue:
How to get the ATV312 to restart at the last set frequency after the power has been cycled, when using up and down arrows on the speed reference or when using the plus and minus speeds?

Product Line:
ATV31 and ATV312 drives

Environment:
ATV31 all serial number

Cause:
After a power cycle, when a run command is initiated the drive will run at low speed.

Resolution:
FUN Menu - enter
UPd - Enter
Str = rAn(Save to Ram) - Drive will start at the last set frequency after the run command is cycled
Str = EEP(Save to Eeprom) - Drive will start at the last set frequency after a power cycle
Was this helpful?
What can we do to improve the information ?