Technical FAQs

Ask a Question

Is the CHU361DS provided with a drain screw?

Issue:
Product features

Product Line:
Safety Switches

Environment:
Type 4/4X/5 switches

Cause:
Verification

Resolution:
Yes, a drain screw is provided in the bottom end wall in the back, right corner.
Was this helpful?
What can we do to improve the information ?