Technical FAQs

Ask a Question

What is the terminal lug data for the PKOGTA8 Equipment ground bar used in the 1200amp Heavy Duty Safety Switches ONLY?

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Environment:
Terminal wire sizes

Cause:
application

Resolution:
The terminal lug data for the PKOGTA8 used in the 1200amp HD Safety Switches ONLY, is (8) #4 - 350kcmil Al/Cu wires.
NOTE: the PKOGTA8 kit actually contains 2 ground bars with 4 holes in each bar, to allow for 4 incoming wires and 4 outgoing wires. 
Was this helpful?
What can we do to improve the information ?