Technical FAQs

Ask a Question

Combox system wattage incorrect when AC coupling

Try changing the AC output association on the GT/TX from AC1 to GRID1 (or vice-versa).

When Set to "Grid <1 to 10>":
GT grid output will be added to the system wide grid power.

If the GT grid output association is "AC <1 to 10>":
GT grid output will not be added to the system wide grid power, indicating that the GT is load coupled with XW, so the system wide grid power will not be "doubled".
Was this helpful?
What can we do to improve the information ?