Technical FAQs

Ask a Question

Will the QOMB1, QOMB2 or QOMB3 OEM Mounting Bases accept QOT tandem circuit breakers?

Issue:
Application

Product Line:
OEM Mounting Bases

Environment:
OEM Mounting Base application

Cause:
Verification

Resolution:
No, these OEM Mounting Bases accept only full size QO circuit breakers.
Was this helpful?
What can we do to improve the information ?