Technical FAQs

Ask a Question

What is the length of the GVAPA1 shaft?

Issue:
How long is the GVAPA1 shaft?

Product Line:
GV2 Manual Starters

Environment:
All Product Lines

Cause:
Can not find it in the Digest

Resolution:
The length is 315mm or approximately 12.40"
Was this helpful?
What can we do to improve the information ?