Technical FAQs

Ask a Question

Are enclosure modifications available for the Type 7/9 Safety Switches or Circuit Breaker Enclosures?

Issue:
Product features

Product Line:
Safety Switches and CB Enclosures

Environment:
Product features

Cause:
Clarification

Resolution:
These enclosures are cast aluminum and there are no options for variations to the enclosure features.
Was this helpful?
What can we do to improve the information ?