Technical FAQs

Ask a Question

Can LC1K contactors be operated in any position?

Issue:
Can LC1K contactors be operated in any position?

Product Line:
K-Line Mini Contactors:
LC*K contactors

Environment:
US Product

Cause:
Space requirements may require alternates to traditional mounting position.

Resolution:
Attached is the operating position guide showing acceptable mounting positions.  Note that certain positions will require derating the contactor.
 
Was this helpful?
What can we do to improve the information ?