Technical FAQs

Ask a Question

If the Irrigation Field drive comes with a circuit breaker does it require external fuses feeding it?

Issue:
Circuit protection question

Product Line:
8930 Irrigation Field drive

Environment:
Class 8930

Cause:
None

Resolution:
The Irrigation field drive comes with their own short circuit protection devices.  They do not require additional external short circuit protection.
Was this helpful?
What can we do to improve the information ?