Technical FAQs

Ask a Question

Where can I find XW+NA PDP AC power distribution bars for multi-unit 120/240VAC installations?

The XW+ Installation Guide (975-0239-01-01 Rev G Pg.1-7) shows (4) distribution bars are included with 865-1020-01, but the quick start guide for connection kit (975-0708-01-01 Revision A) in section F indicates this connection kit is to have breakers purchased separately so the part # 865-1020-02 will apply to NA models and Euro models. Future revisions of XW+ Installation Guide should be edited to reflect this.
THE ONLY PART # THAT INCLUDES DISTRIBUTION BARS IS (865-1215-01). See attached.

Note : These bars are NOT available for purchase separately.
Was this helpful?
What can we do to improve the information ?