Technical FAQs

Ask a Question

What is the IP rating or NEMA rating for XY2CE cable pull switches?

Issue:
What is the IP rating or NEMA rating for XY2CE cable pull switches?

Product Line:
XY2CE Preventa Safety Cable Pull Switchs

Environment:
US Product

Cause:
These switches may be installed in environments which are wet or dusty

Resolution:
The XY2CE cable pull switches are rated IP65, but they do not have a NEMA rating.
 
Was this helpful?
What can we do to improve the information ?