Technical FAQs

Ask a Question

ATS22: what is the input current in reference to the output current ?

Issue:
On the ATS22, what is the input current in reference to the output current ?

Product Line:
ATS22

Environment:
 All

Cause:
Installation / Setup

Resolution:
It should be the same. Input current = output current.

Was this helpful?
What can we do to improve the information ?