Technical FAQs

Ask a Question

Why won't my Combox upgrade firmware on some devices?

There are slight differences between file names for older legacy XW models and the newer XW legacy models
or the  XW+NA models. 
Older firmware file names may have the model # followed by ".01", for example one revision of older SCP firmware
would be (865-1050.01_05_00.BN0001.xf0). For the Combox to recognize the firmware, it will be necessary to rename the file 
to (865-1050-01_05_00.BN0001). In other words, just change the "dot" to a "dash".
Was this helpful?
What can we do to improve the information ?