Technical FAQs

Ask a Question

Why does the 4000 amp SE breaker have two 1.0 longtime pickup settings?

Issue:
Why does the 4000 amp SE breaker have two 1.0 longtime pickup settings?

Product Line:
SE circuit breaker

Environment:
4000 amp only

Cause:

Resolution:
On the 4000 amp SE breaker the .95 setting was eliminated.  They needed to fill the empty position on the dial so it has two 1.0 settings. See attached photo.
Was this helpful?
What can we do to improve the information ?