Technical FAQs

Ask a Question

What are the limitations for AC coupling XW+

AC Coupling with XW+ Models

The Comments from Escalation state that for AC coupling you can AC couple up to the lessor of (2 X power rating of single XW+) or 48A relay parameter(48*240=11.5kw)

Example:With (2) XW6848+ total power would be 13.6 kw, and with the 48amp transfer relay (48*240=11.5kw)
Answer:The grid tie inverters would have to be set at or less than 11.5kw since 13.6kw is above the 48 amperage parameter.

 
Was this helpful?
What can we do to improve the information ?