Technical FAQs

Ask a Question

Where can I locate the firmware version for the ATV12 drives?

Issue:
Where can I locate the firmware version for the ATV12 drives?

Product Line:
ATV12 Drives

Environment:
All serial numbers for ATV12 Drives

Cause:
N/A

Resolution:
The firmware version can be located on the silver plate attached to the side of the drive.
The plate should also include the drive model number and serial number

Was this helpful?
What can we do to improve the information ?