Technical FAQs

Ask a Question

Are 9065 solid state overloads phase sensitive?

Issue:
Are 9065 solid state overloads phase sensitive?

Product Line:
NEMA 9065 solid state overloads - GIC product

Environment:
US Product

Cause:
Older units were phase sensitive

Resolution:
F series solid state overloads can be used with single phase applications.  The hot leg must be looped so that the overload senses current through all three openings.
Was this helpful?
What can we do to improve the information ?