Technical FAQs

Ask a Question

Can the ATV32 go into local mode?

Issue:
Can the ATV32 go into local mode?

Product Line:
ATV32 Drives

Environment:
All serial numbers for ATV32 Drives

Cause:
N/A

Resolution:
Yes the ATV32 keypad can go into local mode. 
However it does not have local controls on the front of the drive itself. You would need to connect the HMI keypad (VW3A1101) to put the drive in local mode.

Was this helpful?
What can we do to improve the information ?