Technical FAQs

Ask a Question

What is the difference between the Type PB and Type S Panelboard Lighting Contactors?

Issue:
Product and Application Difference

Product Line:
Lighting Contactors

Environment:
8903 PB and S

Cause:
Use and mounting 

Resolution:
These two types of panelboard contactors mount differently. The standard Type PB has busbar connections whereas the Type S has lugs.  The low profile PB contactors are all mecahnically-held , however the smaller footprint Type S can be electrically or mechanically-held.
 
Was this helpful?
What can we do to improve the information ?