Technical FAQs

Ask a Question

What is AR busway?

Issue:
Need to add to busway AR2520G4ST. 

Product Line:
Busway

Environment::
I-line II

Cause:
Product understanding
 
Resolution:
"AR" indicates aluminum riser busway, that has plug-in ports on one side only. This is also available as CR copper busway and can connect to standard feeder or plug-in products.

Keywords:
I line, bus way, prefix
Was this helpful?
What can we do to improve the information ?