Technical FAQs

Ask a Question

What type of enclosure protection is provided by the Altivar flange kits?

Issue:
What type of enclosure protection is provided by the Altivar flange kits?

Product line:
ATV61 ATV71 VW3A95** flange kits

Environment:
All models

Cause:
Flange kit application

Resolution:
The VFD power section has IP54 degree of protection and can be mounted outside the enclosure utilizing a flange kit.  The kit maintains an Nema Type 12 rating for dust and damp proof enclosures.

 
Was this helpful?
What can we do to improve the information ?