Technical FAQs

Ask a Question

How to order the switch replacement mechanism for 9037 switches?

Issue:
How to order the switch replacement mechanism for 9037 switches?

Product line:
Float switches

Environment:
Applies to 9037 Float switches

Cause:
There is a message saying to supply class and type when ordering

Resolution:
Customer must include the class and type number of the switch when ordering because the switch mechanism includes the cover which has the class and type numbers on it
Was this helpful?
What can we do to improve the information ?