Technical FAQs

Ask a Question

Can the ATS22 an input phase loss be disable in the aTS22 softstarts?

Issue:
Can the ATS22 an input phase loss be disable in the aTS22 softstarts?

Product Line:
ATS22

Environment:
All

Cause:
Custom configuration

Resolution:
Yes , Input Phase detection can be turned by:
Goto Menu Pro
Goto parameter PHL
Set to No
Was this helpful?
What can we do to improve the information ?