Technical FAQs

Ask a Question

How to determine if the Masterpact breaker a fixed type or drawout type?

Issue:
Is the NW breaker fixed type or drawout type?

Product Line:
Circuit Breakers

Environment:
Masterpact NT, NW

Resolution:
If the sixth digit of the Masterpact catalog number in a "R" then it is a drawout type.  Otherwise it is a fixed type breaker.
Was this helpful?
What can we do to improve the information ?