Technical FAQs

Ask a Question

Where can I find spare parts or renewable parts for an M-Flex?

Issue:
Spare or renewable parts

Product Line:
M-Flex

Environment:
All M-Flex enclosed drives

Cause:
None

Resolution:
The 8839 M-Flex instruction Bulletin document number 30072-451-52 contains the renewable parts for the M-Flex.  If a specific part not on this list needs to be replaced then a request needs to be made to Seneca Tag using the Factory Order number.
Was this helpful?
What can we do to improve the information ?