Technical FAQs

Ask a Question

Do you have cable operating mechanisms for the Type LAL, LHL, and Q4L breakers?

Issue:
Do you have cable operating mechanisms for the Type LAL, LHL, and Q4L breakers?

Product Line:
9422 Cable Operating Mechanisms

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
We offer 3 lengths, and with or without the 9422A1 handle operator.

Without Handle:

36" Cable - 9422CLA30
60" Cable - 9422CLA50

With Handle:

36" Cable - 9422CLA31
60" Cable - 9422CLA51
120" Cable - 9422CLA11
Was this helpful?
What can we do to improve the information ?