Technical FAQs

Ask a Question

Can the LX4F8* coils be used on AC voltages?

Issue:
Can the LX4F8* coils be used on AC voltages?

Product Line:
TeSys F-Line Contactors

Environment:
All Product Lines

Cause:
The Digest does not specify

Resolution:
These coils can be used on either DC or AC voltages; however, if you want to use it on an AC voltage, you must use a rectifier DR5TE4U (110-240V) or DR5TE4S (380-440V).
Was this helpful?
What can we do to improve the information ?