Technical FAQs

Ask a Question

What filler plates are used with the CHOM Canadian HOMELINE load centers?

Issue:
Selection

Product Line:
Canadian Homeline

Environment:
Filler plates

Cause:
Selection

Resolution:
The main breaker filler plate is QOM1FP if the panel uses the QOM1-VH main breaker (125A max) or QOM2FP if the panel uses the QOM2-VH main breaker (225A max). The branch breaker filler plate is HOMFP.
Was this helpful?
What can we do to improve the information ?