Technical FAQs

Ask a Question

In an ATV212 where do I enter the motor nameplate current?

Issue:
In an ATV212 where do I enter the motor nameplate current?

Product Line:
ATV212  Atltvar 212
ATV21

Environment:
All

Cause:
Startup

Resolution:
Enter motor current in F415.
Also should enter the motor current in the tHr parameter to make sure the drive provides proper overload protection
Was this helpful?
What can we do to improve the information ?