Technical FAQs

Ask a Question

What does the *01 or *10 indicate at the end of the part number on the K-Line contactors?

Issue:
What does the *01 or *10 indicate at the end of the part number on the K-Line contactors?

Product Line:
TeSys K-Line Contactors

Environment:
All Product Lines

Cause:
The Digest does not specify.

Resolution:
the *10 will indicate a normally open auxiliary contact

the *01 will indicate a normally closed auxiliary contact

(example: LC1K0910 has one normally open auxiliary contact)
Was this helpful?
What can we do to improve the information ?