Technical FAQs

Ask a Question

9007EA11: On the screw that tightens to the arm, what is the diameter?

Issue:
9007EA11: On the screw that tightens to the arm, what is the diameter?

Product Line:
9007 Limit Switches, Heavy Duty Industrial Single and Two Pole

Environment:
9007 switches

Cause:
Assembly

Resolution:
Screw is 8-32 X 1/2"
Was this helpful?
What can we do to improve the information ?