Technical FAQs

Ask a Question

What are the standard control units/pilot devices used on a Model 6 MCC?


Issue:
Standard Push Buttons, Selector switches and Pilot lights

Product Line:
Motor Control Centers

Environment:
MCC6

Cause:
Size and Type of controls

Resolution:
The XB5 22mm devices are standard and 30mm 9001K are optional

Was this helpful?
What can we do to improve the information ?